Other Parts Discussed in Thread: SN6505A
Hello Team,
Attached is the schematic which uses "SN6505AQDBVTQ1" and "750316032" Transformer for having Isolated power from 3.3V to 5V.
I testing the same circuit with physical board.
I'm seeing 0V at the input of the U13 IC.
I was suppose to receive 6.6(1:2).
Is there any thing wrong with the circuit? Please support to resolve this issue.
Thanks