Replies: 1
Views: 34
Part Number: ISO1432
Hi Team,
Customer is doing full-duplex config and wondering if RT needs to be placed on both side end of the bus?
Below we see different picture, so want to double check, thanks.
Andrew
Hi Andrew,
Thank you for reaching out to us!
The termination resistor (RT) should be placed at both cable ends to remove line reflection.
For full-duplex, it has two signal pairs (4 wires) and hence you need four termination resistors as shown
in the below figure.
Regards,
Alfred Chong