How do you generate isolated power for a digital isolator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How do you generate isolated power for a digital isolator?
There are several options to generate isolated power for a digital isolator; the best solution depends on the specific application needs.
One option is to use a transformer driver like TI’s SN6501, which operates in a push-pull configuration with a transformer and optional rectifying low-dropout regulator (LDO) on the secondary side (Figure 1). The SN6501 is capable of delivering as much as 1.5W to provide isolated power. This device has the flexibility for use in almost all applications, because the transformer and turns ratio can provide the necessary isolation rating and output voltage for the power supply. You can use the SN6505 instead of the SN6501 for as much as 5W of output power if you need isolated power for additional devices. SN6505 has extra protection features such as overload and short circuit, thermal shutdown, soft start, and slew rate control enabling a robust solution.
Figure 1: Isolated power for the ISO7741 using the SN6501
Another option for space-constrained applications is the ISOW78xx family of devices, which provides signal and power isolation in a small-outline integrated circuit (SOIC)-16 package. This combination is compact; doesn’t require a transformer; and makes certifications easy. See all documentation available in the ISOW7841 online product folder for more information.
Figure 2: Digital isolator with integrated signal and power using the ISOW7841
All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.
Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.
TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.