Hi Team,
My customer is using the ISO7760F to isolate signals from an FPGA and signal to analog switch.
We’re trying to understand if it’s acceptable to run this part at different Vcc based on each own gnd reference. In the datasheet, all examples are using Vcc1 = Vcc2. For this isolate, is this possible Vcc1 = 2.5V and Vcc2 = 5V? It’s also important to note that GND2 could be up to 60V and GND1 is the system gnd.
Thanks,
Mitchell