This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7760: DC/DC swiching noise interference concerns

Part Number: ISO7760

Hi,

The customer is designing their ISO7760 PCB as below picture:

The big red box is an isolated DCDC REM6E-1711074 in top layer, REM6E-1711074 datasheet is in attached. But in bottom layer small red box is ISO7760.

This PCB board is 2 layer, and there is no copper GND.

Customer want to know whether our ISO7760 will be interfered by isolated DC/DC.

Do you have some suggestions?

REM6E-1711074选择.pdf

  • Hi Rock,

    Thank you for reaching out..

    Since the DC/DC is operating at about 120kHz, I believe it shouldn't be an issue under normal operating conditions. Are there any specific EMC tests that customer is going to run on the DC/DC? If yes, then we recommend customer to conduct those sufficiently to rule out any EMC related issues. Thanks.

    Regards,
    Koteshwar Rao