Hello Team,
We are using SN6506B for an isolated gate drive power supply in a high voltage power supply. The secondary side of the transformer experience a large voltage swing every time the power transistor switches. We are finding dV/dt induced transient voltages occurring at the D1 and D2 pins of the SN6505B that approach the absolute maximum rating of the part (16 V). Are you aware of any clamping or protection techniques that can be used with the SN6505B? We have tried Zener diodes, but they tend to cause heating problems in the SN6505B. We are assuming this is due to the capacitance on the Zener diodes. Thanks for your feedback!
Regards,
Garret