This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH Tools/ISO7720: ISO7720 IBIS

Part Number: ISO7720

Tool/software: WEBENCHRegistered Design Tools

Is there a way to use IBIS data as SPICE DATA?

Or can you tell me some values ​​of the internal circuit?

Isolation barrier capacitor capacity
Vref
Resistor value
OSC oscillation frequency
LPF time constant

Best Regards, BANE

  • Hi Bane,

    IBIS data can be used for simulations with the tools that support use of IBIS models. Please see below E2E post for more details related to IBIS models and the suitable simulation tools.

    Regarding the additional information sought related to device internal circuit, sorry we will not be able to provide this information as this is TI proprietary information. Thanks.

    Regards,
    Koteshwar Rao