This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6505A: Adding CLK while the device is disabled

Part Number: SN6505A

Hi team,

My customer will use SN6505A for his application and he is asking some basic questions.

  1. Is it okay to input clock to CLK pin while the device is disabled as long as CLK pin satisfies rating?
  2. As for sequence for each pins(CLK, EN, VCC), VCC should come first since abs rating of CLK and EN  is <VCC + 0.5V . There is not limitation for sequence of CLK and EN after VCC power-up.
    Is this understanding correct?

Best regards,

Shota Mago