Other Parts Discussed in Thread: ISOW7741, ISOW7841
Hi Team,
Please review the review attached schematics section ISOW7842DWE and SN74LVC1T45DCKRG4.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yaseen:
Thanks for reaching out to us for a schematic review!
I have reviewed your design and didn't see any concerns regarding the device functionality. However, I did observe that you're using a Y-capacitor across the isolation barrier for better EMC performance. You may also refer to this tech note for additional recommendations for low EMI performance.
Alternatively, you may also consider our second generation ISOW7741 for your design. ISOW7741 EMI performance is improved compared to ISOW784x family and can meet CISPR32 Class B with significant margin on our 2-layer EVM.
Please feel free to reach out to me if you have any additional questions.
Regards,
Dushmantha
Hi Yaseen,
Like Dushmantha mentioned, please do consider using ISOW7741 which offers improved EMI performance over ISOW7841 and helps meet your emissions requirements. Additionally, ISOW7741 has provision for supplying separate power DC-DC and IOs thereby allowing the sections to be independently supplied and operated. This will eliminate the need for the two voltage level translator that you have used in your design.
I hope you have all the inputs that you need. I will go ahead and close this post and if you have any further questions, please do not hesitate to respond back. Thanks.
Regards,
Koteshwar Rao