How to calculate the maximum SPI speed supported by a digital isolator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to calculate the maximum SPI speed supported by a digital isolator?
Serial Peripheral Interface (SPI) is a single-master, 4-wire, synchronous, serial communication interface and the 4 signals involved are - SCLK, SDO (MOSI), SDI (MISO) and CS\ (SS\). The master provides the clock, SCLK, to all the slaves and one bit is transferred in each clock cycle. Hence, speed of SPI interface is determined by the frequency of SCLK.
During the rising edge of SCLK, data changes to value that needs to be transmitted and during the falling edge it remains stable so that it can be sampled. This is shown pictorially in the below diagram.
The below diagram shows a typical SPI connection between an SoC and an MCU through a quad-channel digital isolator. The below diagram also shows how propagation delay shifts SCLK as it passes through digital isolator and how it affects data that is being received.
The slave prepares data at the rising edge of SCLK and master samples the data at the falling edge of SCLK. Since data needs to be read in half SCLK cycle and SCLK / SDOI together go through a round-trip propagation delay of digital isolator, the minimum SPI clock period or the maximum SPI speed can be expressed as shown below.
2 * tpd(max) < tSCLK(min) / 2
In other words,
fSCLK(max) < 1 / [ 4 * tpd(max) ]
As an example, let us consider ISO7741 that has a tpd(max) of 16ns for VCC1 = VCC2 = 5V. The maximum SPI speed that can be achieved on ISO7741 is, fSCLK(max) = 15.6 MHz.
All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.
Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.
TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.