Hello team.
One customer considers to use our ISO1211 device in digital input modules for Programmable Logic Controller.
As customer claims, test for IEC 61000-4-6 compliance is mandatory for such kind of end application.
On ti.com we can find tests results on compliance to IEC 61000-4-2, IEC 61000-4-4, IEC 61000-4-5.
But there is no information on IEC 61000-4-6 compliance.
So I have two questions regarding this:
1. Did we perform IEC 61000-4-6 compliance test for ISO1211? Can we provide any materials in case we did?
2. Can we give any design recommendation for successful passing these tests?
Thank you for support in advance.