Hello,
Concerning LM2903QPWRG4Q1 and LM2903AVQPWRG4Q1, I have questions as follows;
So, can I get answer of these questions ?
Question-1
Concerning the Non-A device (=LM2903QPWRG4Q1),
are there any possibility that the device which has 4mV(MAX) Vio
(=Input offset voltage) is included ?
Question-2
Through the LM2903-Q1 datasheet, I could not find the
temperature dependency data of the Vio.
If the Ta(=Ambient Temperature) becomes lower, Vio value becomes
higher or lower ?
Thanks and best regards,