This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPA3110D2-Q1: Vp and PLIMIT

Genius 4135 points

Replies: 1

Views: 452

Dear all,

Could you teach me the individual difference and tolerance over temperature (-40~85C) of Vp?

**Please consider PLIMIT has no tolerance

You mentioned 'Vp=4*PLIMIT' at data sheet.

However, is this '4 times' always the same value between devices or temperature?

We think that this value changes to '4.0xx' or '3.9xx' between some situation.

If our think is wrong, what does this '4 times' derive from?

In addition, could you teach me how tolerance should we think if you don't have clear answer?

Best regards,

  • Yamamoto-san,

    This is specified in the datasheet; it is the last line item on page 5. For a VPLIMIT = 2V, the output voltage maximum can be between 6.75V and 8.75V. If you turn that into a gain, the gain can be between 3.375 and 4.375.

    Thanks,

    -Clancy

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.