Dear TI-er.
TLE4275-Q1 is input voltage 45V(Datasheet 1page, operating max 42V(datasheet 3page).
Can TLE4275-Q1 operate input voltage 55V 400mS ?
How I protect it ?
Can you recommand protect circuit ?
plz help me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI-er.
TLE4275-Q1 is input voltage 45V(Datasheet 1page, operating max 42V(datasheet 3page).
Can TLE4275-Q1 operate input voltage 55V 400mS ?
How I protect it ?
Can you recommand protect circuit ?
plz help me.
Dear TI-er.
TL751M05-Q1 is 60V LoadDump Protection.
Is it for 24V automotive battery system(input min 24V ~ max 32V) ?
plz help me.
Hello ElSalvador,
TLE4275 may be able to handle 55V load dump; however, this is not something that TI can guarantee since it is past abs max spec. As suggested, TL751M05 is a good alternative.
From the datasheet, Vi (max) is 26V. Therefore, a 24V battery system will be ok to handle a 60V load dump. The device may be able to handle 60V load dump with Vi = 32V; however, once again, this is not something TI can guarantee since it is not within the datasheet limits.
Best Regards,
Wen-Shin Wang