Hello,
can some body show me a power switch as an TPS2054B for 5V, now with about ~35Volt (less or more)
I need a shortprotectet treiber with 0,5 A or more by ~35V DC with up to 8 chanel. Outputs with erros by overload will be graet.
Thanks
Thorsten
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
can some body show me a power switch as an TPS2054B for 5V, now with about ~35Volt (less or more)
I need a shortprotectet treiber with 0,5 A or more by ~35V DC with up to 8 chanel. Outputs with erros by overload will be graet.
Thanks
Thorsten
Hey,
not 5A! only 0,5A up to 1A.
it is for switching Turnouts in a Modellayouts. The Custemers often do mistakes in the cabiling or the turnouts have a problem. I youse the ULN2803 thats works but by mistakes they are not protakted.
http://www.can-digital-bahn.com/modul.php?system=sys5&modul=8#Mod_Top
Thorsten
Our product area does not have this type of device. A couple of things closer to what you might look for areTPIC2603 or LMD18400. I will transfer this to a fourm that might be closer.
We don't have any power switches in Industrial Interface, I will move this to the forum that supports the TPIC2603.
Hello Thorsten,
Please take a look at our LMD18400 Quad High Side Driver datasheet (attached) and let us know if it meets your application needs and if you have any questions.
Best Regards,
-Juan
Hello Juan,
the LM18400 looks verry good but the price! This one with 8 Chanels will be great.
normaly i need only the short and overvoltage protektion, all other is nice to have
I will try the TPIC2603, but as an special solution i test the LMD18400 or do you now same parts with 8 Channels?
Thanks for the help
Thorsten
Hello Juan,
i hope some other one writes me a 8 Chanel Idea. Has TI no other one with 8, 500mA per chanel will be enough or must i post it in a other Forum?
Thanks
Thorsten