This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65381 SEL_VDD3/5 pin



Today in a design review some of the senor engineers got a bit nervous about the statement in the TPS65381 datasheet concerning the SEL_VDD3/5 pin needs to be a "no connect" for 3.3V operation and wanted to pull it up to some voltage to prevent potential problems with noise issues at start-up.


I'm reluctant to do such since it is a violation of the datasheet and was tasked with digging into this further.

Can anyone tell me more about this pin?

Is there a internal pull-up source, if so how strong?

Can it be pulled up externally, if so to what voltage?