My application requires me to put a CAN transceiver in the circuit. The MCU communicates with the CAN transceiver through a Digital Isolation Barrier IC - ISO7241C. My input supply is from a Battery operating at 24V.
I have used a Buck Converter, TPS57040-Q1, 500mA step-down SWIFT DC/DC Converter to step down to 5V. This 5V power rail supplies directly to a Push-Pull Transformer Driver, SN6501-Q1, to create an isolated line for the CAN transceiver. The isolated 5V supply rail directly connects to a bqSWITCHER battery Charger, bq24105-Q1, which is a switch-mode battery charger for a Li-ion Backup cell.
Since all of these switching supplies will be operating at much different switching frequency, I would like to ask if there are any precautions I should be taking ? I had initially thought of putting LDOs in between 2 switching supplies to reduce the output ripple to the next input, but that seems to be a very costly affair. Please feel free to give me any solution that seem fit.
- Tapajit.