Hello,
I want to use this DC/DC for a 48V-to-12V step-down application. The 48V input will 99.9% of the time be <58V but we have a very specific 70 transient test to survive shown in the attached figure. Since the part is rated for Abs Max Vin=60V, I am concerned that it would not survive this test. Do you think the part would survive this 70V transient test?
Thank-you!