Hi,
I am trying to develop a reflective ultrasonic distance measurement solution. I need to measure distances ranging from about 5cm on the low end, up to about 100cm maximum. I'm primarily looking for maximum precision (<1mm) and high measurement update rates (>10Hz).
My understanding is that it is not possible to measure distances less than about 10cm using a single transducer configuration due to ringing. My question is whether there is any issue with using separate Rx and Tx transducers with the PGA450 to get around this issue. If this is possible, could the EVM be hacked to facilitate development with a dual transducer configuration?
I'm also curious about what transducers would work best for my application and if it is even possible to hit my specs but that may need to be a different thread.
Thank you for your help,
Gabe