I am powering a low power MCU (3.3v) and ADC (5v ref) from a switched 12v supply, with a dirty 5v standby supply. My current implementation is to use the TPS65320 running a 5v buck, and a 3.3v LDO. Running off 12v, this gives a clean 5v (after additional filtering) and 3.3v rail.
I'd like to use one of the TPS211xA power muxes to switch between the standby rail and buck output. We tried applying an input voltage to only VIN_LDO using a diode-OR configuration, and appeared to fry the PMIC. I'm not sure if this was a bench error, or if the auto-sourcing circuitry was not made to be operated in this fashion. Are there any foreseeable issues with this approach?
(I didn't see anything in the datasheet about operating them separately)
Thanks.