This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS70950-Q1 and TPS7A6950-Q1/TPS7A6950-Q1 Vo Accuracy

Other Parts Discussed in Thread: TPS709-Q1

Hello,

 

Please advise if following my understand for Vo accuracy when Io=5mA and full temperature range is correct or not.

 

TPS70950-Q1:

Datasheet specifies Vo accuracy is +/-1% max at Io=1mA, and Load regulation is 50mV max while 100uA<Io<150mA. So worst case accuracy at Io=5mA is follows.

 

  Vo accuracy max = +1%

   Vo accuracy min = -1% -(50mV/5V) = -2%

 

TPS7A6950-Q1/TPS7A6950-Q1:

Datasheet specifies Vo accuracy is +/-2% at Io=1mA to 150mA.

 

  So worst case accuracy at Io=5mA is +/-2%.

 

Please advise which LDO is better accuracy at Io=5mA.

 

Best Regards.