Hi team,
Could you please answers for the following question related to UCC2805-Q1 max rating?
1. Absolute max rating voltage of VCCis 12V in datasheet. And 13.5V is clampped in the block diagram. So could you please clarify which voltage is absolute max voltage over all temp condition?
2. If the Vcc voltage maintains 18V during 100msec, what happens? Is it damaged or not?
3. What voltage are absolute max voltage for other pins(COMP, REF, OUT, RT pins)? There are only CS and FB in the datasheet.
Thanks,
WS