Hi Team,
I am evaluating the TPS61240-Q1 for the following specs:
Input: 3.3V
Output: 5V @ 600mA
Now, when I look in the datasheet, at 3.3V input, it looks as though this part will not work for 600mA output:
However, when I run a webench design, it looks as though this part can run at those specs:
I am inclined to believe that the webench simulation is actually more accurate since my input voltage is not that low as compared to the output voltage, but will need evidence that the part can handle the 600mA output current.
Please let me know if the webench is actually reflecting the correct value of output current and please let me know where in the datasheet I should be looking to fully understand output current capabilities.
Thank you,
Jared