This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[ SN74LVC1G126-Q1 ] Tpd distribution and/or statistical data

Other Parts Discussed in Thread: SN74LVC1G126, SN74LVC1G240, SN74LV125A, SN74LVC1G126-Q1

Hi,

Do you have a data which express the typical value, distribution and/or statistical data of Tpd?


Thank you for your support in advance.
Regards,
Ken

Other reference post.
SN74LV14APWR, SN74LV125A, SN74LVC1G240 and SN74LVC1G126 - tPLHD and tPHLD typ value
https://e2e.ti.com/support/logic/f/151/t/447537

  • Hi Kenichiro,

    What voltage are you planning to operate at?

    For now I can refer you to the Typical Charactersitics section on page 7 of the SN74LVC1G126 datasheet. There you will find two plots that show tpd for various load capacitance. This is the non-Q1 version but the parts are essentially the same.

    Hope this helps.

    Regards,

    Joe
  • Hi Joe,

    It's good information! Thank you.
    I have shared the information from non-Q1 with my customer.

    He would use SNLVC1G126-Q1 with 3.3V power supply.
    It's great if you have specific data for this condition.

    Thanks,
    Ken

  • Hi Joe,

    Do you have any further information on this??

    Thanks,
    Ken
  • Hi Ken,

    The Q1 version is essentially the same part as the non-Q1, so the figures on page 7 of the the SN74LVC1G126 datasheet are accurate and can be used. This data was tested for 3V +/- 0.3V.

    How is the part going to be operated? You mentioned 3.3V power supply, but are there other operating conditions that need to be concidered, such as temperature? Is there a maximum propagation delay for the system that the customer is worried about?

    Depending on the load capacitance the part sees, the typical propagation delay can range from ~2.5 ns to ~7.5 ns (low to high transition) and ~2ns to ~5ns ( high to low transition).

    Please provide more detail.

    Thank you,

    Joe
  • Thanks, Joe,

    I just wanted to know whether you have anything specific information for SN74LVC1G126-Q1. It's okay, I have asked customer to check the information on the datasheet of SN74LVC1G126 (non-automotive) as reference.

    Thank you for your support!
    Regards,
    Ken