This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65311-Q1: Closed window time

Part Number: TPS65311-Q1

Hi,

Closed window time is mentioned typical value(=twd/4) only. on the datasheet

However the twd is guaranteed min/max value.

Actually, is closed window time guaranteed(min:18/4=4.5ms max;22/4=5.4ms)?

Best Regards,

Kuramochi