This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Linux/PROCESSOR-SDK-AM57X: UDP Throughput Queries

Genius 12965 points

Replies: 5

Views: 990

Part Number: PROCESSOR-SDK-AM57X

Tool/software: Linux

Hi,

I have a customer who is interested in UDP throughput of Sitara devices with Linux SDK.
We found below Wiki site and it shows some data.

http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Kernel_Performance_Guide?keyMatch=performance&tisearch=Search-EN#UDP_Throughput

But it is not clear number of A15 cores used for AM57xx (1 or 2).
And how much CPU load is needed. (For TCP Throughput, CPU load is shown)

Could you provide the information ?

Thanks and regards,
KoT

  • Hi KoT,

    This is the officially released kernel performance data.

    We do not have publicly available data for cpu load, when benchmarking the ethernet.

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Hi Yordan,

    OK, I understood no CPU load data are available.

    But we should know number of CPU cores used for AM572x at least.

    Thanks and regards,
    KoT

  • In reply to Koichiro Tashiro:

    I believe the performance guide indicates the dual cortex a15 load, but lets wait on the factory team to confirm.

    Best Regards,
    Yordan

     


     Please make sure you read the forum guidelines first.

  • In reply to Yordan Kovachev:

    Hi, KoT,

    The performance is done using iperf with the following command "iperf -c <server_ip> -P 2 --format m -u -b <bandwidth/2>M --len <packet_size_in_byte> -t 60"

    SMP Linux will distribute those 2 threads in different cores.

    Rex

     

  • In reply to Rex Chang:

    Hi Rex,

    Thanks!
    I am not familiar to iperf, but I understood two streams are used and each thread is distributed to each core (total 2 cores are used).

    Thanks and regards,
    KoT

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.