Other Parts Discussed in Thread: Z-STACK
Tool/software: Linux
We have downloaded Z-STACK-LINUX-GATEWAY and trying to compile it on Ubuntu 16.04 64-bit linux platform. We are able to compile main.bin file and when launched it shows following. But we dont have documentation on using this file.
usage: ./main.bin <nwk_mgr_hostname> <nwk_mgr_port> <gateway_hostname> <gateway_port> <ota_hostname> <ota_port> [<log_filename>]
We also tried to replace existing precompiled main.bin with the new one in app folder, and tried to execute zigbeeHAgw as follows, but got erros
$> ./zigbeeHAgw x86
file NPI_lnx_x86_server is missing
file ZLSZNP_x86 is missing
file GATEWAY_SRVR_x86 is missing
file NWKMGR_SRVR_x86 is missing
file OTA_SRVR_x86 is missing
there are 5 missing files!
exiting ./zigbeeHAgw
Could you please provied detailed instructions on compiling above files? Where is the source code for above binaries? I dont think it is part of installer Z-Stack_Linux_Gateway_1_0_1_installer.run avialble to download. Somewhere I read about signing LCA with Local TI. If yes, please provide details of Local TI in India. I hope after signing SLA, we get something other than Z-Stack_Linux_Gateway_1_0_1_installer.run
regards,
--
Satish