Tool/software: Linux
Hi,
I am working with Processor SDK 3.4.
I want a small system but it has to have a 3D accelerator support.
Using the big File system it has way too many things that I do not need.
Using the base file system, I cannot find rc.pvr in the init folder. It looks like its not part of the small file system.
What would be the procedure of adding it?
Is it through menuconfig of the linux and then building.
Or is it a separate package that has to be compiled and then installed on the target?
Kind regards,
Ugnius