Hi,
I want to run Audio codecs on C66x DSP of Jacinto 6 (DRA7xx).
Currently libdce supports only VIDDEC2, VIDDEC3 and VIDENC2 interfaces.
Can anyone guide me how to add AUDDEC1 interface support to libdce?
Things I tried till now:
I am able to rebuild the DSP server (dsp_vidsvr) using dspdce_1_00_00_04 and run the copycodectest example on target.
I am also able to run an auddec1 codec on the DSP by converting the VIDDEC2 calls/parameters coming from an ARM application (similar to copycodectest.c) to AUDDEC calls/parameters on the DSP server (in dce.c of dspdce_1_00_00_04).
Now I want to make direct AUDDEC calls from ARM side application. Hence I need to add AUDDEC1 interface support in libdce.
Please guide how it can be done.
I am using GLSDK 6.10.00.04.
Regards,
Abhishek