This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Does TI support 2-bytes data format on matrix function?

Intellectual 500 points

Replies: 12

Views: 12378

Hi, all
On EVMK2H12, I used "cblas_sgemm" from Processor-SDK to calculate large matrix. I know the interface has been optimized based on OpenCL on 8 DSP cores. But the result is not satisfied according to performance requirement.

I've checked the performance for M=N=K=1000, it is 0.027s as same as TI said (www.ti.com/.../linear-algebra-libraries.page

However when the values are large such as M=10,N=200,000,K=30, it is 0.277s. Well, maybe this kind of calculation has reached the limit of performance for all DSP cores. So I think it could be improved if the input data format is short or fp16 (half precision float-point), which is 2 bytes length instead of 4 bytes like float.

Does anyone know if the SDK supports sgemm with 2 bytes data format? I didn't find anything by searching SDK manual and cblas.h. If not, is there any plan on this topic for TI?

BTW, I had used fp16 data format on matrix calculation based on NVIDIA platform, which improves performance significantly (NV supports fp16 in CUDA library)

Thanks very much for any help on this topic!

  • In reply to jianzhongxu:

    Sorry, one clarification: Given all these factors, sgemm may not be running with optimum speed for this specific matrix size.
  • In reply to jianzhongxu:

    Thanks for your information, jianzhong!

    All the things is clear in my side now.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.