This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OpenMP accelerator on evm-k2h: Is it possible to use only part of the DSP cores?

Expert 1280 points

Replies: 0

Views: 1366

Hi, 

I am currently looking at the OpenMP accelerator examples provided within the Processor-sdk-linux package. If I understand correctly, the target portion of the example is pushed to all DSP cores. 

Is there a way to limit or specify which cores can be used for OpenMP operations?

In my application, I need one of the cores to run a Sys/Bios application and would like to use the other cores as OpenMP accelerators for codec processing. Would that be possible?

Regards,

- David