This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

I want to do the simple image processing using ti chip.

Prodigy 140 points

Replies: 1

Views: 2883

hello

I have used the ti chip like tms320f28xx to run motors. I always got helps and advisements from here to do it.

These-day i want to do some simple image processing. 

Just crop the images from two camera and merge it as one image.

If I do this on MATLAB or openCV, it is very easy, but this time I have to do this on the embedded system which i don't know much.

So I ask you, which chip is good to it, and is there some paper for me to refer?

Thank you

 

 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.