This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6638K2K, CCSv6, Pro Trace Memory Transaction Logs shows wrong EDMA_CC

Hello, 

We capture memory transaction logs via XDS560v2 Pro Trace with the settings below:

We modified the settings for capturing DSP1 LSRAM (L2_1) EDMA WR Access only.

Our application uses EDMA_CC1_TC0 for default, and we confirmed this with the logs. But when we modify the application for using EDMA_CC4_TC0 instead of EDMA_CC1_TC0, even though the register&paramset movements confirm that we are using the EDMA_CC4_TC0, memory transaction logs show that we are using EDMA_CC2_TC0.

Moreover, there is no EDMA_CC4 in the transaction master list below.

So far I am sure that there is no paramset in EDMA_CC2 which addresses DSP1 L2SRAM as destination. We are using CCS Version: 6.1.1.00022. Any suggestions about that?

Thanks in advance..