This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 781
Hi,
As i check from the dataheet of UC1823A, it has %100 maximum duty cycle of each output.
1) Are two PWM outputs of UC1823A in phase?
2) Does each output have %100 maximum duty with same phase?
3) Can i drive the mosfets of 2xseparete buck converter with one UC1823A (by using high side gate driver IC)?
4) What is the difference between UC3823A and UC1823A?
5) What does highlighted sentence mean at the attached figure?
Thank you.
Waiting for responses,thank you.
In reply to gG:
In reply to Ramesh Khanna: