Do we have an IBIS model for the ADS5474-SP? It is not shown in the current product folder.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do we have an IBIS model for the ADS5474-SP? It is not shown in the current product folder.
Hi Steve,
Please use the IBIS model for the ADS5463 which appears on the product page of the ADS5474.
As described by apps engineer supporting these devices:
"The ADS5474 and ADS5463 are essentially the same device for purposes of the ibis model. The ADS5474 has an extra two LVDS outputs which may not be listed in the pin list. The main differences between the ADS5463 and ADS5474 are that the analog input circuit is tweaked between them to optimize for their respective sampling rates, but the analog inputs are not ibis-modeled. So not an issue. Also, one of the devices has a VCM pin and the other doesn’t – but again not part of an ibis model which is meant for the digital IO."
Regards,
Christian
Wade -
Have we updated the IBIS model to account for the ceramic package yet? Please advise