Posting for a customer. For the TLK2711-SP, please help to address the following questions related to the Icc spec.
From the Datasheet: http://www.ti.com/lit/ds/symlink/tlk2711-sp.pdf page 8 table 7.3.
VDD: Voltage supply spec’d at 2.5 +/-5%
- What is the spec for VDDA?
- Can this be relaxed, as it is specified to be L-C decoupled from VDD supply, and will be lower on average.
Icc: Supply current is 110 mA nominal @ 1.6 GHz.
- What is a min & Max spec for this current? Is this at 25 C, or over the MIL temp range?
- What is the split in current between VDD and VDDA pins?
- If not a spec, can you provide any typical data for Icc(Vdd) and Icc(Vdda)?
- What is the dependence of Icc on VDD Supply voltage? (Linear, or?)
- What is the dependence of Icc on Temperature?