This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

SM320C6727B-EP: Need AC Overshoot / Undershoot Specifications

Intellectual 2275 points

Replies: 1

Views: 283

Part Number: SM320C6727B-EP

Hello,

We have a customer who is requesting the AC Overshoot / Undershoot specs.

Could someone please help track this down?

Thank you,

Gabe Garza

TI Customer Support

Gabe Garza
TI Technical Support

  • Gabriel,
    We do not have overshoot/undershoot specifications for this device.
    However, there are 2 specifications that can help define this.
    1) The absolute maximum ratings for voltage input range. This is specified as -0.3 to DVdd +0.5 (excluding clock).
    and
    2) the input clamp current. This is typically labelled IIK, but in this datasheet is it just labeled Clamp Current. This is specified at /-20mA.

    To prevent violating the absolute max conditions, the signal would need to stay within -0.3 to DVdd + 0.5V.
    If it exceeds this, its current must be less than the clamp current to prevent damage to the device.
    Proper termination and potentially series resistance for current limiting.

    Regards,
    Wade

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.