This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 981
Part Number: OPA4872-EP
Hi
I intend to use OPA4872-ep as a video multiplexer as a replacement of Max440. Is it recommended for video multiplexer? From the spec it looks that it can be used as a video multiplexer?
Does video multiplexer has some special characteristics? I consider OPA4872 can be used as video multiplexer but can you please comment on it.
Also i need to cascade two multiplexers as a 8:1. I want to short A1 pin of two multiplexers and drive it from a host microcontroller. Will it be a problem?
Regards;
In reply to Christian Yots:
In reply to Raheel Bari: