Hello
Could you please help answer the following question from one of my customers
‘We currently use Digital Signal Processor part SM320F2812PGF-EP in one of our applications. The core and I/O supplies are powered from tight tolerance linear voltage regulators providing 1.9V and 3.3V respectively. These regulators have voltage supervisors that would assert the DSP reset line if the voltages fall outside a defined region, for example if one of the regulators fails to regulate. We power the core at 1.9V to allow operation at 150MHz.
Under worst case tolerances the reset line would be asserted when the supply voltage is already outside the specified operating conditions in the DSP datasheet:
DSP datasheet I/O supply voltage range: 3.14V to 3.47V
DSP datasheet Core supply voltage range: 1.81 to 2.0V
Worst case assertion of the reset line by the 3.3V voltage supervisor: low end 2.998V; high end 3.655V
Worst case assertion of the reset line by the 1.9V voltage supervisor: low end 1.74V; high end 2.11V
Specifically we would like to know if the DSP would degrade its operation or completely misbehave if it were powered at the extreme voltages quoted above. Our testing at these voltages indicates no impact at all but obviously we cannot see what happens inside the processor.’
I think the main point is how much leeway is given beyond the recommended operating conditions. The figures above of course a worst case conditions if something went wrong. How are the recommended limits worked out?
Regards
Bob Bacon