Part Number: TPS50601-SP
The last response in this thread stated that, after an external sync signal is applied, if it is later removed, the TPS50601-SP will not switch back to using the internally-generated sync signal. If that is true, then what does it do? Does it just stop functioning?
Another question: the datasheet states that "When operating the converter in internal oscillator mode ..., the synchronous pin becomes the output". This contradicts Table 1 in the datasheet. Elsewhere in the datasheet it states that the sync pin is an output only in master mode, which is when the RT pin is left unconnected. So my question is this: is the sync pin ever an output when there is a resistor connected from the RT pin to AGND? I'm concerned that there could be contention between the externally-supplied sync signal and the internally-generated sync signal both trying to drive the sync pin simultaneously especially at the point when operation switches from the internal sync signal to the external sync signal.
Thanks,
Jerry Molisani