Dear Sir/Madam
Can anyone suggest me with some standard EMI filter IC that can be used in the PLL section of SMJ320C6701-SP processor?
Regards
Akash JB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir/Madam
Can anyone suggest me with some standard EMI filter IC that can be used in the PLL section of SMJ320C6701-SP processor?
Regards
Akash JB
Akash,
There is an application note that shows clocking for various C6000 DSPs.
http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=spra430a&fileType=pdf
Within this app note, TDK and Panasonic EMI filters are referenced.
The 3.3-V supply for the EMI filter must be from the same 3.3-V power plane supplying the I/O
voltage, DVDD. In multiple-C6000 designs, it is important to provide a separate EMI filter circuit
to each DSP. Multiple chips on a single filter will not work properly. The DSP will not function
properly (except in x1 mode) without an EMI filter. The EMI filter used in the figures below is
TDK part number ACF451832333, 223, 153, 103 or Panasonic part number EXCCET103U.
I am not familiar with Class V equivalents.
Regards,
Wade