After completing a design it was found that the absolute maximum ratings on the TL331-EP comparator were being exceeded in 2 operation modes for the system. The maximum rating lists the input voltage for V+ or V- as -0.3V.
Mode 1: V+ = -5.3V, V- = 0V, Vcc = 0V
Mode 2: V+ = -3.9V, V- = 0.4V, Vcc = +20V
For these 2 modes what would the failure mechanism be for the device?