Hi
I have been evaluating the TPS62110HT to 175C and found the VOUT drifted from 1.85V at 25C to 2.05V at 175C for RLOAD 10K to 10R. I tested with VIN=5V, 10V and 12V.
Between 150C to 175C it goes from 1.87V to 2.0V.
I checked the datasheet and to my surprise there is no drift parameter or chart for HT and EP datasheet.
Is there way to fix the drift issue? it connect to SM320F28335 device.
Regards