Hi,
We are currently building an amplifier which must work across a wide range of temperatures, ideally up to 200°.
We would like to use the TLE2426 or something similar to generate a split rail supply from our single ended supply. Is there any information on the behavior of the TLE2426 above 125° or are there any alternate parts which may be suitable?
The sink/source current from the virtual ground will be <= 5ma.
Cheers,
Mike