Hi,
One of my customers is using the ADS4245-EP in a parallel CMOS output format at 15Msps. The datasheet mentions the output setup and hold time on the parallel interface starting from 65Msps in Table 3 on page 15. Since this application is at 15Msps, can I extrapolate the data from the list as setup time to be 40% of T and hold time to be 42% of T and arrive at 26ns rise and 28ns hold time?
Is there actual data available?