Other Parts Discussed in Thread: SN7407
Can any one please suggest the alternate part number for SN5407.
Open drain output current - 40ma
High level output Voltage - 30V
Temperature - 40V to +125.
Thanks
Arulmurugan P
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Wade,
Thank you for your reply
SN5407 is through hole part and in the same version SN7407 is SMD part but temperature is 0 to 70C.
We are looking for SMD components with same specification of SN5407. ( 40ma, High output voltage - 30V)\
Regards
Arulmurugan
Unfortunately there is not device with higher rating.
The design is the same between the SN7407 and SN5407, just different package, testing, and qualification screening.
If you operate the SN5407 within the SN7407 temperature range, then 40ma will be possible without damaging device.
Regards,
Wade