Other Parts Discussed in Thread: SN74LVC04A
Hi,
It is specified in SN74LVTH125-EP datasheet that continuous maximum current into the output pin (low state) as 128mA. So,for the given 4 outputs can i load upto 512mA
at most or Is there any limitaion on supply pin / ground pin current? which is not specified in the datasheet. I want to use this buffer for high-speed PWM driving.what is the maximum frequency i can go for?
Thank you.