Hello,
The TPS50601-SP datasheet says in section 8.3.10:
"If an external Schottky diode is used from VIN to boot, then a bleeder may be required <1 mA to ensure output is low when the unit is disabled by EN pin."
Where is this bleed resistor needed? On the BOOT pin? On the PH output node (before/after inductor)?
Thanks,
Chris