This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM301A-N: Question about slew rate

Genius 4075 points

Part Number: LM301A-N

Hi,

I found the description about the slew rate of LM301A-N in D/S page1(FEATURES) and Page13(Figure39 and 40).

Does anyone have the operating characteristic data of slew rate of LM301A-N  at specified conditions? (like page7 in TL031 D/S )  

Thanks

Go

  • Go,

    LM301A has far more detail about slew rate than TL031 has. For TL031 slew rate is fixed and independent of the passive components around it (up to a point of course).

    LM301 is more complicated as it has two extra pins for AC performance tweaking.

    There are three basic setups; single pole, two pole, and feedforward. See figure 17, 18, 19.
    The slew rate for each is buried in figures 26, 27, 28.

    For example single pole (fig 26) has a NSLEW of 5V in 10uS = 0.5V/us. PSLEW is same, however there is a much faster PSLEW start