Part Number: LT1014-MIL
Other Parts Discussed in Thread: LT1014, LM124AQML
5962-89677022A (LT104)
Question1) Part Number 5962-89677022A (LT104) Related Questions
What happens on the part when + 15V DC is input to VCC (+) and GND is input to VCC (-)?
1. In this case, whether the output value is + 14V, GND
In addition, is there any other problem with the output?
2. Does the range of input value differ from the normal range of LT1014 when GND is input to VCC (-). ?
3. Are there any additional problems in addition to normal operation?
Question2)
1. Is there a Military grade OP-Amp that can be used with + 15V DC to VCC (+) and GND to VCC (-) among TI's products?